Componentes electrónicos
Manténgase un paso adelante
Automatización industrial
Automatización industrial al alcance de su mano
(Source: HARTING)
Wiring was once treated as a practical detail, something to be addressed once the mechanical design was complete. Machine design has become highly modular, with integrated networking enabling plug-and-play functionality. Power, signal, data, and even pneumatic connections are essential to modern machine architectures and directly affect performance and uptime.
Wiring and connection strategies directly affect assembly, long-term reliability, and maintenance. As we enter an era of remote diagnostics, connections can also determine whether a machine can support predictive maintenance. In this blog, we discuss how planning for connectivity early in the design process using modular connectors helps improve assembly, reduce errors, and support scalable, serviceable systems suited for data-driven and autonomous operation.
Despite this transition, many designs still treat wiring as a final step, with associated costs often becoming apparent during assembly and commissioning. Without planning, control cabinets become congested, and cable routing is forced into whatever space remains. Documentation can struggle to keep pace with last-minute changes, creating complexity that is difficult to manage and easy to get wrong.
Traditional hardwiring techniques often create additional problems as machines become more modular. Higher I/O density means more conductors, more terminations, and more opportunities for error. Each connection must be made individually, and often under time strain. The manual nature of the assembly process increases the risk of miswiring. Errors often become obvious only when the power is switched on. Fixing the problem leads to delays, downtime, and added cost.
How machines are serviced once in use is also affected by late-stage wiring decisions. Installations that rely on fixed wiring require more time to modify or repair. Fault-finding can be time-consuming, and replacing components requires skilled labor on-site. With the latest distributed systems, “on-site” can mean remote and inaccessible, incurring yet more cost and delay.
Replacing point-to-point wiring with plug-and-play interfaces is part of a larger trend. Rather than building systems wire by wire, engineers are adopting pre-engineered assemblies that can be installed quickly and consistently.
Pre-terminated harnesses reduce labor requirements and eliminate much of the variability associated with manual wiring. Pre-assembled connections are far less prone to error. Installation becomes a process of mating interfaces rather than terminating conductors, keeping commissioning time to a minimum.
Connectorization also simplifies the machine’s physical layout. Instead of routing separate cables for power, signal, and data, these can be consolidated into fewer interfaces, simplifying cable management.
These benefits extend across the equipment lifecycle. Faster installation and fewer wiring errors lower upfront costs, but improved serviceability lowers the total cost of ownership. Connector-based approaches can be more practical and reduce lifecycle costs in applications where installation time, maintenance, and changeover flexibility are important.
Modularity takes the practical advantages of connectors further by combining multiple transmission types within a single interface. Rather than specifying separate connectors for power, signal, data, and pneumatic hardware, these elements are integrated into a single compact solution.
Modular connectors employ a building-block approach. Individual components are selected based on their function. They are then arranged in a common housing to form a connector that meets the application’s requirements. The concept is straightforward, but the impact on design flexibility is significant.
By combining different media in a single interface, engineers can reduce the overall footprint of the connection system while simplifying installation and maintenance. Modular connectors also support scalability. Additional functions can be introduced by reconfiguring the connector rather than redesigning the entire wiring scheme. For machines operating in demanding environments or for installations subject to frequent changeovers, this flexibility is particularly valuable.
As industrial systems become more autonomous, connectivity becomes more critical because lights-out or minimally attended operation depends on consistent signal integrity, reliable power delivery, and uninterrupted data flow, particularly when systems are monitored remotely. Any weakness in the connection system can compromise the entire process.
Well-designed connector interfaces help maintain this reliability. Secure connections reduce the likelihood of intermittent faults and ensure that critical data continues to flow. Accurate information is essential for remote diagnostics, as it enables the identification and resolution of issues without direct intervention, supporting predictive maintenance.
Connectorization supports faster fault recovery. Connectors use mechanical keying to prevent incorrect mating. In the case of modular connectors, each interface can be made unique by changing the order in which functions are arranged, preventing mating errors. Modularity also supports the upgrades through quick-disconnect designs that allow components to be replaced rapidly.
Taking a more structured approach to connectivity does not require a complete redesign of existing practices, but it does mean making decisions earlier in the design process.
Connectivity should be defined alongside the mechanical design. Power, signal, data, and pneumatic paths should be identified early, allowing routing and interface decisions to be made before space becomes limited.
Environmental conditions must also be considered from the outset. Connectors are among the few components mounted on the exterior of equipment, and factors such as vibration, moisture, and temperature must be taken into account. The right housing and locking mechanism can significantly influence long-term reliability.
The final consideration is how the design will accommodate change. Because machines represent significant investments and cannot be replaced frequently, they can be updated to leverage new technologies. Whether the system requires new sensors, controllers, or actuators, building flexibility into connector selection early in the design process can help avoid extensive rewiring later.
Extending this flexibility into implementation, HARTING’s Han‑Modular® Connector System helps replace late-stage hardwiring with a more streamlined, plug-and-play approach. By enabling engineers to consolidate power, signal, data, and even pneumatics into a single, compact, and coded interface, it reduces the late‑stage integration challenges and hardwiring complexity that can otherwise slow progress and introduce errors. The result is a connectivity approach that is easy to assemble, error‑proof to mate, and fast to service, helping cut installation and commissioning time, reduce footprint, and improve uptime in modular machines.
In parallel, Han‑Modular aligns closely with the trajectory of modern industrial systems—supporting modular machine design, ongoing miniaturization, and the demands of Industry 4.0 and IIoT data capture. Its integrated and reliable connectivity underpins lights‑out operation and predictive maintenance, while enabling faster deployment, safer operation, and more sustainable outcomes across advanced manufacturing environments.
The transition from hardwiring to modular connectivity is already underway. As equipment gets more compact and more capable, the limitations of traditional wiring are becoming clearer.
By addressing connectivity early in the design process, engineers can simplify installation, improve serviceability, and create systems that are better suited to modern manufacturing requirements. Being able to combine multiple transmission types within a single interface, as seen in solutions such as HARTING’s Han-Modular Connector System, further enhances flexibility, supporting modular design and reducing overall complexity.
As the demands on connectors grow, driven by increased automation, higher data volumes, and evolving performance expectations, modular approaches provide a foundation that allows machines to adapt without major redesign, helping to ensure that today’s systems remain capable of meeting tomorrow’s challenges.
David Pike is well known across the interconnect industry for his passion and general geekiness. His online name is Connector Geek.
HARTING develops, manufactures and sells electrical and electronic connectors, device terminations, backplanes, network components as well as cable harnesses for networks or machinery, or for power and data application in factories. HARTING products are used in mechanical and plant engineering, broadcast and entertainment, factory automation, power generation and distribution as well as industrial electronics and telecommunication