Authorized Distributor Mouser Electronics Spotlights Latest from Bourns in Circuit Protection, Transformers and More

Para publicación inmediata

Comuníquese con nosotros


June 13, 2023Mouser Electronics, Inc. is shipping the latest innovations from Bourns®, a leading manufacturer of automotive sensors, circuit protection solutions, microelectronic modules, precision potentiometers and resistive products. Offering world-class solutions in virtually all industries, Mouser continues to expand its customers’ product development process by stocking more than 20,000 parts from Bourns. Additionally, Mouser.com hosts a growing collection of Bourns eBooks, resources and other technical content.

Bourns PLN planar transformers are forward converter transformers designed for 48 W to 70 W Power over Ethernet (PoE) industrial applications, that require a low profile with a high power density, like battery management systems (BMS). Bourns PLN planar transformers, available from Mouser, operate at a switching frequency of 250 kHz and voltages from 5 V to 12 V with an output current from 4 A to 14 A, making them perfect for both power management and LED lighting applications.

For high voltage applications, Bourns Model BID insulated gate bipolar transistors (IGBTs), combine technology from a MOSFET gate and a bipolar transistor for high voltage/high current applications like switch-mode power supplies (SMPS), uninterruptible power sources (UPS) and power-factor correction (PFC). The Model BID IGBTs are thermally efficient, utilizing advanced trench-gate field-stop technology to provide greater control of dynamic characteristics, resulting in lowered collector-emitter saturation voltage and fewer switching losses.

The Bourns MF-ASML/X low-resistance PPTC resettable fuses, also available from Mouser, utilize a proprietary freeXpansion™ design to increase performance with higher hold currents, higher voltages, and improved resistance stability in a small (0402) footprint. Designed to protect against both overcurrent and overtemperature events within space-constrained mobile applications, such as battery charging and USB port protection, the Bourns MF-ASML/X PPTC resettable fuses offer plug-and-play protection for PC motherboards as well.

For high-temperature environments, Bourns MF-FSHT PTC resettable fuses offer a 12 V voltage rating, up to 40 A input current rating, and a low profile (0603) design. MFFSHT fuses feature surface mount packaging for automated assembly, a maximum operating temperature rating of +125°C, and low thermal derating factor. The Bourns freeXpansion design increases fuse performance, making them ideal for industrial and other demanding applications required to operate at elevated temperatures.

Partnering with Bourns since 2007, Mouser has received multiple top performance awards in recent years from Bourns, including e-Commerce Distributor of the Year award for 2022, 2021, 2019, 2018, 2015, 2014 and 2012, as well as 2016 Distributor of the Year (Catalog Partner) in EMEA, 2012 European Distributor of the Year POS Growth Award, and the 2012 Asia Distributor of the Year POS Growth Award.

To learn more about the wide selection of Bourns products available from Mouser Electronics, visit https://www.mouser.com/manufacturer/bourns/.

To review the selection of Bourns eBooks, visit https://www.mouser.com/manufacturer/bourns/ebooks/.

 

Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.

Acerca de Mouser

2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.

Acerca de Bourns

2026 - Bourns is a leading manufacturer and supplier of automotive sensors, circuit protection solutions, magnetic products, microelectronic modules, trimming and precision potentiometers, panel controls, encoders, and resistive products. Headquartered in Riverside, CA, Bourns serves a broad range of markets, including telecommunications, computer, industrial, instrumentation, automotive, consumer, non-critical life support medical, audio, and various other market segments. Bourns products are manufactured according to ISO-9000 standards under Six Sigma quality programs. Bourns automotive products are manufactured in accordance with IATF 16949.

Marcas

Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.

Para obtener más información, comuníquese con:
Kevin Hess, Mouser Electronics
Vicepresidente general de Marketing
+1 (817) 804-3833
Para consultas de prensa, comuníquese con:
Kelly DeGarmo, Mouser Electronics
Gerente, Comunicaciones Corporativas y Relaciones con los Medios
+1 (817) 804-7764