Mouser Electronics Signs Distribution Agreement with BreadBoard Mates to Deliver Development Display Technologies
November 30, 2022 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, announces a new global distribution agreement with Breadboard Mates, a leading supplier of micro-LCD-displays for breadboard and electrical development projects. Breadboard Mates’ Tiny Intelligent Modular Instrument (TIMI) hardware and Integrated Development Environment (IDE) software products are designed to replace and simulate component readouts and meters that demand extensive hardware resources for breadboard or electronic development projects.
Mouser is now stocking the latest BreadBoard Mates products, including the TIMI-96 display development module. The TIMI-96 incorporates hundreds of built-in widgets, allowing design engineers to streamline development projects using fewer components at lower cost. The TIMI-96 display development module is a 160 × 80, 0.96” TFT LCD module featuring a 4D Labs PIXXI-28 graphics processor for stand-alone, host-driven interfaced, PC-tethered, and educational applications.
The TED-96 display module is the OEM version of the TIMI-96 module, designed for product integration where the TIMI-96 may not be suitable. The TED-96 is a 0.96” TFT In-Plane Switching (IPS) LCD module also driven by the 4D Labs PIXXI-28 graphics processor. The module includes both castellated and through-hole pads at each end to allow for different mounting options. Various interfaces arm the TED-96 with resources to be either a stand-alone controller, a host-driven secondary device, or a tethered instrument while being able to interface with and power external devices. For larger displays, Mouser offers the BreadBoard Mates TIMI-130 — a unique breadboard-compatible display development module with a 1.3” TFT IPS LCD (40 × 240) display. The TIMI-130 features a unique MatesBus interface, which is simple to use in breadboard applications, adapters, or directly into products. The main TIMI-130 interface is a 3.3 V level asynchronous serial UART featuring three GPIOs that can be used as digital or analog inputs, digital outputs, master I²C communication, or PWM audio output.
The TIMI-MB display development module provides a simple interface display solution for boards and modules that include MikroBUS sockets. The TIMI-MB module is a 0.96” TFT LCD with a five-pin programming header that programs its processor using the Mates Programmer, a selection switch that alternates between programming modes or connection to the MikroBUS host. The TIMI-MB module is a flexible design aid for demanding hardware resources for breadboard and electronic development projects.
To learn more about the BreadBoard Mates products now available from Mouser Electronics, visit https://www.mouser.com/manufacturer/breadboard-mates/.
Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.
2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.
About Breadboard Mates
2026 - Breadboard Mates was established in October 2020 to bring breadboard-friendly products to the market, significantly reducing the time and components required to develop and experiment with electronics. From hobbyist to engineering professional, Breadboard Mates cutting edge products can be utilized for seamless development with the help of the integrated products like TIMI (Tiny Intelligent Modular Instrument) and the Mates Studio software development tool. Mates Studio is unlike any other, offering four different programming methods with a library of hundreds of pre-designed pages and widgets. The result is an unprecedented increase in development speed for stand-alone, host driven or PC testing applications.
Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.