Mouser Electronics Signs Global Distribution Agreement with EnOcean for Sustainable IoT Solutions
April 5, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, announces a new global distribution agreement with EnOcean, the pioneer of energy harvesting devices and sensor-to-cloud solutions for sustainable Internet of Things (IoT) applications. EnOcean’s family of tools and interfaces for Smart Building applications simplifies the commissioning and integration of control networks in IoT systems based on the ISO/IEC 14908-1 Local Operating Network (LON) protocol and other open standards. EnOcean provides solutions that facilitate integration of LON devices with energy harvesting EnOcean devices for building automation, smart homes, lighting control, industrial applications, and more.
LON network design is made easier using the new EnOcean IzoT™ Commissioning Tool (CT), available at Mouser Electronics. The EnOcean IzoT Commissioning Tool allows designers to draw networks using the integrated Microsoft Visio tool, automatically configuring communication with LON devices and matching their configuration to the drawing. The result is a network drawing that becomes the "as-built" documentation for the network that is a critical deliverable from the building integrator to the building owner. IzoT CT integrates any LON devices including LON/IP, LON/IP-852, LON/IP-FT, LON/IP-TP-1250, LON-FT, LON-TP-1250, and LON-PL devices.
The EnOcean U60 FT and U60 TP-1250 DIN USB network interface expansion modules enable a SmartServer™ edge server, embedded controller, or computer to communicate with LON free topology (FT) or 1.25 Mbps (TP-1250) twisted-pair networks via USB. The U60s facilitate communication with everyday devices like pumps, motors, valves, sensors, actuators and lights for lighting controls, building automation, energy management, transportation systems control and telecommunications equipment management. The U60 compact devices are available in DIN 43880 2TE-compliant enclosures and interface with LON/IP-FT, LON/IP-TP-1250, LON-FT, and LON-TP-1250 networks.
EnOcean U60 FT USB network interface modules allow an embedded controller or computer to communicate via USB with LON/IP-FT and LON-FT networks. These compact boards include network and USB pin headers for quick integration into any controller or device. The source code for LON/IP protocol stacks and U60 drivers is available at no charge from EnOcean at www.github.com/izot.
The EnOcean U70 PL-20 USB network interface expansion module allows a SmartServer edge server, an embedded controller, or any computer to communicate via USB with LON PL-20 power line carrier networks. The U70 facilitates communication with everyday devices communicating via power line networks such as street light controls for Smart City applications. The U70 PL-20 compact module is engineered in a DIN 43880 7TE compliant enclosure compatibles.
To learn more about the EnOcean products available from Mouser Electronics, visit https://www.mouser.com/manufacturer/enocean/.
Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.
2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.
2026 - EnOcean provides valuable data for the Internet of Things (IoT) with its resource-saving energy harvesting technology. EnOcean produces maintenance-free wireless switches and sensors, which gain the device's energy from the surrounding – from movement, light, or temperature. The combination of miniaturized energy converters, ultra-low power electronics, and robust radio technology based on open standards (EnOcean, Zigbee®, and BLUETOOTH®) forms the foundation for digitized buildings, services, and production processes in the IoT. EnOcean's self-powered solutions are used in building automation, smart homes, lighting control, and industrial applications.
Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.