Mouser Electronics and Efficient Power Conversion (EPC) Enter Global Distribution Agreement to Deliver High-Performance Power Solutions
May 18, 2026 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, today announces a global distribution agreement with Efficient Power Conversion (EPC), a global leader in enhancement-mode gallium nitride (eGaN®)-based power solutions, offering GaN devices spanning 15 V to 350 V. EPC's eGaN FETs and integrated circuits deliver performance far beyond that of the best silicon (Si) power MOSFETs in applications including DC-DC converters, remote-sensor technologies such as lidar, motor control for e-mobility, robotics, drones, and more.
The agreement is aimed at expanding access to GaN technology for engineers worldwide and accelerating the adoption of high-efficiency power solutions.
"This global agreement with Mouser is part of our distribution strategy to engage with more engineers who are looking at designing with GaN because of the benefits it offers over silicon," said Nick Cataldo, Senior VP Sales & Marketing of EPC. "Mouser has a fantastic global reach, and we are excited to be partnering with such a dynamic company."
"EPC's portfolio of high-performance power solutions is a strong complement to our line card and aligns well with the needs of our customers," said Heather McGriff, Vice President of Supplier Management for Mouser. "We're excited to build a successful long-term relationship and bring these innovative technologies to the global engineering community."
The EPC2302, now available from Mouser, is a 1.8 mΩ max RDS(on), 100 V eGaN power transistor in a low-inductance 3 x 5 mm QFN package with an exposed top for excellent thermal management. It is designed for high-frequency DC-DC applications from 40 V to 60 V and for 48 V BLDC motor drives. The exposed top enhances top-side thermal management, and the side-wettable flanks ensure the entire side pad surface is wetted with solder during reflow, protecting the copper and enabling soldering on this external flank for easy optical inspection. The ultra-low capacitance and zero reverse recovery of the eGaN FET enable efficient operation in many topologies. Performance is further enhanced due to the small, low-inductance footprint.
The EPC2304 eGaN power transistor is designed to handle tasks where ultra-high switching frequency and low on-time are advantageous, as well as those where on-state losses dominate. The device is well-suited for motor drives, class D audio, wireless power, and power factor correction (PFC) converters. The EPC2304 is offered in a 3 x 5 mm thermally enhanced QFN package with an exposed top and ultra-low thermal resistance for cooler operation. The package also features wettable flanks to simplify assembly and inspection.
The EPC23102 ePower™ Stage IC integrates an input-logic interface, high-side level shifting, synchronous bootstrap charging, and gate drivers, along with eGaN output FETs, into a single monolithic integrated circuit in an MSL1 QFN package, using EPC's proprietary GaN IC technology. The result is a power stage IC that translates logic-level control signals into a high voltage and high current power stage, which is simpler to design, smaller in size, and easier to manufacture, plus more efficient to operate. This device is ideal for motor-drive inverters, class-D audio amplifiers, half-bridge and full-bridge LLC converters, and more.
The EPC2305 is a 150 V eGaN power transistor that delivers lower switching losses and lower gate driver losses than the best-in-class Si MOSFETs, enabling higher power density through its enhanced efficiency, smaller size, and higher switching frequency, resulting in smaller inductors and fewer capacitors. Typical applications for the EPC2305 include phones, notebooks, gaming PCs, power tools, home robotics, e-mobility, and solar.
To learn more about EPC products available from Mouser, visit https://www.mouser.com/manufacturer/epc/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.
2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.
2026 - EPC is the leader in enhancement mode gallium nitride (eGaN®) based power management. Founded in 2007 by experts in power electronics, semiconductors, and business management, the company leverages cutting-edge technology to advance the field of power electronics through the development and commercialization of GaN-based power devices. eGaN FETs and integrated circuits provide performance many times greater than the best silicon power MOSFETs in applications such as DC-DC converters, remote sensing technology (lidar), motor drives for eMobility, robotics, and drones, and satellites.
Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.