Mouser Expands ESD Protection Range with Innovative Solutions for Consumer, Industrial, Telecoms and Automotive Designs
July 23, 2024 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, continues to expand its portfolio of electrostatic discharge (ESD) protection components.
With the constant advancement and miniaturization of electronic devices, ensuring effective ESD protection has become more vital than ever. The incorporation of ESD protection measures serves to guarantee the sustained dependability of devices while safeguarding against immediate, latent, or catastrophic harm to electronic components as a result of an ESD event. Protection components have become an integral aspect of modern electronics and play a vital role in safeguarding delicate electronics against ESD in a diverse array of applications, from consumer electronics, such as smartphones and laptops, to industrial equipment and automotive systems.
Mouser offers a range of new ESD protection products, including the following:
- With the automotive world witnessing a surge in electrification and digitalization, the importance of ESD protection cannot be overstated. The ESD2CANx-Q1 ESD protection diodes by Texas Instruments are AEC-Q101 qualified solutions rated to dissipate contact ESD strikes as specified by the ISO 10605 automotive standard. They feature a 36V working voltage and 2.8pF typical low IO capacitance per channel with a pin-out to suit two automotive controller area network (CAN) bus lines (CANH and CANL). These protection diodes offer long-term protection for in-vehicle networks (IVNs) like CAN-FD, low fault-tolerant CAN, and high-speed CAN systems, as well as in industrial control networks like DeviceNet and CANopen.
- Both wireless and wired communication play a crucial role in the interconnectivity of our modern digital world. The PESDxVF1BALS-Q bidirectional ESD protection diodes from Nexperia are ultra-low capacitance ESD protection diodes that are designed to support communication applications such as NFC, antennas and high-speed data lines. These diodes offer ESD protection of up to ±15kV as per IEC 61000-4-2 standards, and their compact 1mm x 0.6mm x 0.47mm size makes them ideal for designs with limited space. The wide -55°C to +150°C ambient temperature range and AEC-Q101 qualification also make them suitable for harsh environments such as automotive applications.
- The AQ1205-01UTG bidirectional discrete TVS diodes by Littelfuse are made using its exclusive silicon avalanche technology. These diodes have versatile applications, such as automotive use, battery protection and management systems, computers and associated peripherals, medical equipment, consumer electronics, and test instrumentation. With the AQ1205-01UTG TVS diode, circuits can safely absorb repetitive ESD strikes of ±30kV (contact and air discharge) as per IEC 61000-4-2 standards without experiencing any performance degradation. The diodes have a reverse leakage current of 20nA (at a voltage of 4.5V) and a maximum capacitance of 9pF. They are also AEC-Q101 qualified and production part approval process (PPAP) capable, ensuring a smooth integration into suitable designs.
- The PE1403M1Q diode from PANJIT Semiconductor is an ESD protection device in a compact DFN1006-2L package. It features low leakage current, ultra-low capacitance, a 0.88Ω dynamic resistance, and low clamping voltage. The diode suits a wide variety of electronic applications where it can provide protection against lightning-induced voltage transients in accordance with IEC 61000-4-5, as well as protecting against EFT effects and ESD strikes of ±18kV in air on ±15kV in contact. The PE1403M1Q ESD protection diode is fully compliant with EU RoHS 2.0, ensuring it is lead-free, and the diode’s terminals are solderable according to MIL-STD-750, method 2026, allowing for reliable installation.
In Q2 2024, Mouser launched over 10,000 new parts ready for shipment. To see more new innovative products, visit https://info.mouser.com/new_products/.
Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.
2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.
Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.