Mouser Electronics New Product Insider: Over 9,000 New Parts Added in First Quarter of 2026
April 15, 2026 – As an authorized distributor, Mouser Electronics, Inc. is focused on the rapid introduction of new products and technologies, giving customers an edge and helping speed time to market. Over 1,200 semiconductor, electronic component, and industrial automation manufacturer brands count on Mouser to help them introduce their products into the global marketplace. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each manufacturer.
Last quarter, Mouser launched more than 9,000 part numbers ready for shipment. Some of the products introduced by Mouser from January through March 2026 include:
- STMicroelectronics STM32C5 Arm® Cortex®-M33 Microcontrollers
The STM32C5 microcontrollers (MCUs) from STMicroelectronics are specifically designed to boost the performance of billions of tiny smart devices across factories, homes, cities, and infrastructure while meeting stringent cost, size, and power constraints. Based on ST's proprietary 40 nm manufacturing process, the STM32C5 MCUs can run tasks noticeably faster than many entry-level chips currently in use. This gives products more room to include features such as improved sensing, smoother control, and enhanced user experiences while keeping dynamic power consumption low. The MCUs also integrate security features that help safeguard products against tampering and cyber risks. - EDATEC ED-CM0NANO Single-Board Computer
The ED-CM0NANO is a single-board computer (SBC) from EDATEC, based on the Raspberry Pi Compute Module Zero (CM0). The ED-CM0NANO features a quad-core Arm Cortex-A53 processor running at up to 1 GHz, a Broadcom VideoCore-IV graphics processor, and a wide range of connectivity options. Optional Wi-Fi® support with an external antenna enables wireless connectivity, while integrated real-time clock (RTC) and watchdog timer enhance system reliability. These features make the ED-CM0NANO ideal for industrial control systems and Internet of Things (IoT) applications. - Sensata Technologies MGD Resonix™ Refrigerant Leak Sensor
The MGD Resonix™ sensor from Sensata delivers high accuracy and fast response times in a compact module designed to fit into the most compact heating, ventilation, air conditioning (HVAC), and refrigeration equipment. The MGD series offers superior resistance to overexposure and poisoning, as well as to high temperatures (working temperatures up to 105 °C) and humidity. These devices also have a service life of more than 15 years with no need for calibration, making them the ideal leak-detection component for A2L HVAC and refrigeration systems. - u-blox ANN-MB3 Triple-Band GNSS Antenna
The ANN-MB3 antenna from u-blox is a best-in-class L1/L2/L5 triple-band RTK real-time kinematic (RTK) solution ideal for the F20 high-precision GNSS platform. Optimized for seamless integration, the ANN-MB3 antenna delivers exceptional performance with a robust design. The antenna's compact (62 × 80 × 25.5 mm) form factor and flexible installation options enable the adoption of high-precision positioning technologies across industrial, automotive, and robotics applications.
To see more of the New Product Insider highlights, go to https://info.mouser.com/new_products/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.
2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.
Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.