Mouser Announces New Global Distribution Agreement with Phoenix Mecano for Specialty Enclosures and Accessories

Para publicación inmediata

Comuníquese con nosotros


August 28, 2023Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, announces a new global distribution agreement with Phoenix Mecano, a global leader in the enclosure and industrial component segments. Phoenix Mecano's suite of enclosures and accessories covers a wide array of applications in the electronic, industrial, automotive, medical, safety, measurement, and control sectors.

Phoenix Mecano produces both standard and specialized products, which can be customized to the customer's specific application. Mouser now offers many of these enclosures, including:

  • ROSE Polyester standard enclosures provide protection for equipment against certain acids, oils, and fats in food and chemical industries. These robust enclosures are lightweight, high in mechanical strength and impact resistant up to 7J (joules) per EN 60529. ROSE Polyester standard enclosures feature a universal structure suitable for installing terminals and other electronic components, enabling use as a classical terminal enclosure or a distribution enclosure.
  • ROSE Aluminum standard enclosures, designed for mechanical engineering and automation technology, offer IP66 ingress protection and fixing options for DIN rails and mounting plates, making them ideal for the installation of electrical and electromechanical components, including buttons, terminals, switching elements, and electronic modules containing PCBs.
  • ROSE NoVoTronic electronics enclosures feature an aluminum profile enclosure system with IP65 ingress protection for data, PC, and MCR technology operating in -40°C to +90°C temperature environments. These enclosures are offered in a stylish deep black color with ruby red accents and feature external screw channels to ensure reliable protection of electronics and to prevent metal fragments from damaging highly sensitive electronics during assembly. ROSE NoVoTronic enclosures feature integrated guide grooves that function both as a styling and functional element, for slide-in strips or electromechanical components, with built-in stacking and footing aids to ensure secure connections of multiple enclosures.
  • BOPLA Euromas series is a classic industrial enclosure that is available in three different material variants: ABS, polycarbonate and polycarbonate with UL 94 V-0 flame protection. A transparent cover allows a view into the enclosure. Inside the enclosure features large processing areas and versatile mounting options for connectors, switches and keys. Circuit boards can be securely fixed in the base by means of screw domes. The enclosure can also be supplied on request with quick-release fastener screws.

To learn more about Phoenix Mecano, visit https://www.mouser.com/manufacturer/phoenix-mecano/.

 

Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.

Acerca de Mouser

2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.

About Phoenix Mecano

2026 - The Phoenix Mecano Group is a global player in the enclosures and industrial components segments and is a leader in many markets. It is geared towards the development and manufacturing of niche products and system solutions, employing around 8,000 people worldwide.

Phoenix Mecano North America (headquartered in Frederick, Maryland) is a sales, technical support, and custom manufacturing arm of the Swiss global giant, Phoenix Mecano Group. We manufacture industrial components as well as an extensive line of watertight enclosures in Aluminum (cast and extruded), Fiberglass, Polyamide, Polycarbonate, ABS, and Stainless Steel. These durable enclosures are ideally suited for industrial and electronic applications such as instrumentation housings, modular tabletop, machine control, and hand-held enclosures. Through the Rose Industrial Enclosures, BOPLA Electronic Enclosures, and RK Rose+Krieger product lines, Phoenix Mecano has led innovative manufacturing for more than four decades.

Marcas

Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.

Para obtener más información, comuníquese con:
Kevin Hess, Mouser Electronics
Vicepresidente general de Marketing
+1 (817) 804-3833
Para consultas de prensa, comuníquese con:
Kelly DeGarmo, Mouser Electronics
Gerente, Comunicaciones Corporativas y Relaciones con los Medios
+1 (817) 804-7764