Mouser Announces New eBook Showcasing Fundamental Motor Control Design Challenges and Solutions from Qorvo
June 19, 2025 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, announces a new eBook in collaboration with Qorvo featuring industry experts providing key insights into methods, power efficiency and integration solutions available for motor control applications. As solutions in mobility, automation, and robotics have exploded in the past decade, motor-based systems have become a central focus for system designers.
In 10 Experts Discuss the Fundamentals of Motor Control, engineers from Qorvo and other industry leaders offer their perspectives on how Qorvo is helping meet the design challenges of the rapidly evolving motor control environment. Among the topics are the latest in vector (FOC), trapezoidal, sensor and sensorless control solutions, brushless DC motor (BLDC) and permanent magnet synchronous motors (PMSMs). The eBook also includes convenient links to select motor control products Qorvo offers to serve diverse high-growth segments of large global markets, including automotive, consumer, and industrial.
Qorvo ACT72350 motor drivers, available from Mouser, are optimized for driving medium voltage tri-phase BLDC/PMSM motors. These 160V drivers are interfaced through the tri-phase inverter PWM control input signals via SPI and are fully equipped with Qorvo's proprietary, highly configurable Power Manager. The Configurable Power Manager (CPM) provides an "all-in-one" efficient power management solution for multiple types of power sources. The Application Specific Drivers (ASPD) are 180V designed for H-bridge, 3-phase and general purpose driving.
The PAC55710 72V BLDC motor controller and driver is a full-featured, highly optimized System-on-Chip (SOC) that expands Qorvo's portfolio of Power Application Controller® (PAC) products. The PAC55710 controls and powers next-generation smart energy appliances, devices, and equipment with integrated safety features such as VDS sensing, Cycle By Cycle (CBC) current limiting, enhanced Sample and Hold (S&H) for precise estimation, and a Windowed Watchdog Timer for software safety compliance.
The PAC5527 48V charge pump motor controller and driver is optimized for high-speed motor control and driving for small-form-factor battery-powered BLDC motors. It integrates a 150MHz Arm® Cortex®-M4F 32-bit microcontroller core with a highly configurable Multimode Power Manager, Qorvo's proprietary and patent-pending Configurable Analog Front-End™ and Application Specific Power Drivers™.
And finally, Qorvo's PAC52723EVK1 evaluation kit is a complete hardware solution allowing designers to evaluate and develop power applications for the PAC52723, a powerful and versatile Arm® Cortex®-M0 based microcontroller. The PAC52723 microcontroller supplies up to 32 kB of embedded FLASH and 8 kB of SRAM memory, a high-speed 10-bit 1µs analog-to-digital converter (ADC) with dual auto-sampling sequencers, 5V/3.3V I/Os, flexible clock sources, timers, a versatile 14-channel PWM engine, and several serial interfaces.
To read the new eBook, visit https://resources.mouser.com/manufacturer-ebooks/qorvo-10-experts-discuss-the-fundamentals-of-motor-control-mg. To browse Mouser's entire manufacturer eBook library, visit https://resources.mouser.com/manufacturer-ebooks/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.
2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.
Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.