Renesas Electronics’ RA8T1 Arm Cortex-M85 Microcontroller, Now Available at Mouser, Delivers High-Performance Motor Control

Anuncio de nuevos productos

Comuníquese con nosotros


April 10, 2024Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the RA8T1 Arm® Cortex®-M85 microcontroller (MCU) from Renesas Electronics. The RA8T1 MCU meets modern motor control demands, offering high performance, low power consumption, and intelligent operation. The RA8T1 MCU delivers precise motor control for applications including building and industrial automation, smart home devices, and medical equipment.

The Renesas Electronics RA8T1 MCU, now available at Mouser, features a 480MHz Arm Cortex-M85 core with Helium™ technology that provides up to a 4X performance boost for digital signal processor (DSP) and machine learning (ML) implementations over the Cortex-M7 core. The efficient, high-performance MCU is suitable for use in AI predictive maintenance applications that detect anomalies and reduce costly downtime. The RA8T1 Microcontroller offers up to 2 MBytes of code flash memory with dual-bank, background and SWAP operation, 12 KBytes of data flash, and 1 MByte of SRAM with Parity/ECC. The microcontroller features an Ethernet MAC controller, USB 2.0 full-speed, and advanced analog functionalities, making it a highly adaptable solution for a variety of precise control tasks. In addition, the RA8T1 MCU is equipped with a range of analog and communication peripherals for increased adaptability and functionality. The MCU includes advanced security features such as leading-edge cryptographic algorithms, TrustZone, Secure Boot, and immutable storage.

The RA8T1 microcontroller is supported by the RA8T1 evaluation boards and the Renesas Flexible Software Package (FSP). The FSP enables faster application development by providing all the infrastructure software needed, including multiple RTOS, BSP, peripheral drivers, middleware, connectivity, networking, and security stacks, as well as reference software to build complex AI, motor control and cloud solutions. It allows customers to integrate their own legacy code and choice of RTOS with FSP, thus providing full flexibility in application development. Using the FSP eases the migration of existing designs to the RA8T1 device.

To learn more about the Renesas Electronics RA8T Arm Cortex-M85 microcontroller, visit https://www.mouser.com/new/renesa/renesas-ra8t1-microcontrollers/.

 

Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.

Acerca de Mouser

2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.

Marcas

Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.

Para obtener más información, comuníquese con:
Kevin Hess, Mouser Electronics
Vicepresidente general de Marketing
+1 (817) 804-3833
Para consultas de prensa, comuníquese con:
Kelly DeGarmo, Mouser Electronics
Gerente, Comunicaciones Corporativas y Relaciones con los Medios
+1 (817) 804-7764