Mouser Offers Bosch Sensortec’s BHA250 and BHI160 Low-Power Sensor Hubs for Smartphones and Wearables

Anuncio de nuevos productos

Comuníquese con nosotros


Mouser Offers Bosch Sensortec’s BHA250 and BHI160 Low-Power Sensor Hubs for Smartphones and Wearable

November 15, 2016 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the BHA250 low-power sensor hub and BHI160 ultra-low power sensor hub from Bosch Sensortec. Designed specifically for always-on sensor applications in smartphones running the Android operating system, the BHA250 and BHI160 enable designers to offload sensor processing from the main processor, which can reduce power consumption and extend battery life.

The Bosch Sensortec BHA250 and BHI160 sensor hubs, available from Mouser Electronics, integrate a best-in-class 3-axis MEMS accelerometer (BH250) or 6-axis gyroscope/accelerometer inertial measurement unit (BH160) with the new Bosch Sensortec digital signal processor, Fuser Core. The Fuser Core is a 32-bit floating-point microcontroller optimized to execute Bosch Sensortec's sensor fusion and activity-recognition algorithms with ultra-low power consumption — up to 95 percent less than that of other microcontrollers.

The BHA250 and BHI160 are specifically designed for applications in Android smartphones — implementing a full Android sensor stack inside the devices to provide a flexible, low-power solution for always-on motion sensing and sensor data processing. In both devices, the 32-bit Fuser Core microcontroller features 96 kBytes of ROM, including the BSX sensor fusion library, and 48 kBytes of RAM for additional drivers, local data buffering, or feature updates. The devices provide up to three general-purpose input/outputs (GPIOs) and a high-speed I2C interface with data rates up to 3.4 MBit/s for power-efficient data transfer. The devices meet the requirements of smartphones, wearables, and other applications that demand highly accurate, real-time motion data at very low power consumption.

Mouser also offers corresponding shuttle boards for the sensor hubs. Both the BHA250 shuttle board and BHI160 shuttle board, available to order from Mouser, include four external magnetometers that can be connected to the sensor hubs using the available jumpers on the PCB. The shuttle board allows easy access to the sensor's pins via a simple socket and can be plugged into the Bosch Sensortec Application Board.

To learn more about the BHA250 sensor hub, visit http://www.mouser.com/new/bosch/bosch-bha250/. To learn more about the BHI160 sensor hub, visit http://www.mouser.com/new/bosch/bosch-bh160/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated many times daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.

Acerca de Mouser

2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.

Acerca de Bosch Sensortec

2026 - Bosch Sensortec, a subsidiary of Robert Bosch GmbH, has been providing micro mechanical sensors and application services for the consumer electronics market since 2005. Bosch Sensortec has access to the development and manufacturing competencies of the Bosch Automotive Electronics division which makes for flexible and close cooperation during all project phases. This allows not only focus on new applications, but the ability to quickly respond to special customer requests. Due to its integration in the Bosch Group, Bosch Sensortec is capable of a rapid adaptation of existing sensors in new areas of application.

Marcas

Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.

Para obtener más información, comuníquese con:
Kevin Hess, Mouser Electronics
Vicepresidente general de Marketing
+1 (817) 804-3833
Para consultas de prensa, comuníquese con:
Kelly DeGarmo, Mouser Electronics
Gerente, Comunicaciones Corporativas y Relaciones con los Medios
+1 (817) 804-7764