Mouser Electronics Now Stocking Doodle Labs’ U.S. DoD- and NATO-Compliant Smart Radios

Anuncio de nuevos productos

Comuníquese con nosotros


Mouser Electronics Now Stocking Doodle Labs’ U.S. DoD- and NATO-Compliant Smart Radios

September 22, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, stocks the RM-5800, RM-915, and RM-2450 Smart Radios from Doodle Labs. As part of the Smart Radio platform recently contracted by the U.S. Army's Defense Innovation Unit (DIU) and the U.S. Air Force's AFWERX, the multiple-input, multiple-output (MIMO) mesh routers utilize state-of-the-art RF and networking capabilities for faster and reliable communication in drones and mobile robotic systems.

The Doodle Labs Smart Radio platform features self-forming and self-healing Mesh Rider® technology and dependable Mobile Ad-hoc Networks (MANET) that operate in the harshest environments, enabling high-performance radios for real-time video collaboration in the field. The high-speed data links are secure against infiltration, resilient against interference, and frequency agile for global, and interstellar applications. The Smart Radios, available in many frequency bands between 100 MHz and 6 GHz, are capable of carrying out all bi-directional communication (such as command and control and video streaming) in a single high-speed broadband RF channel.

RM-915, RM-2450, and RM-5800 Smart Radios are full-featured 2×2 MIMO radio and mesh routers that provide a long-range, high-throughput data link between one or more mobile units and a control station. The RM-915 (900 MHz) and RM-2450 (2450 MHz) Smart Radios offer a maximum HD video streaming range of 8 km (Pro model) and 20 km (Xtreme model). The RM-5800 radios also offer long-range transmission greater than 100 km, high throughput up to 100 Mbps, and exceptional multipath and near-line-of-sight (NrLOS) MIMO performance.

Doodle Labs' Smart Radios are available in many U.S. Department of Defense- and NATO-specific frequency bands. These routers have gone through a comprehensive process to obtain J/F-12 certifications, so government users can get the Authorization to Operate (ATO) clearance for their projects.

To learn more about the RM-5800 Smart Radios, go to https://www.mouser.com/new/doodle-labs/doodle-labs-rm-5800-smart-radios/. For more information on the RM-915 and RM-2450 Smart Radios, visit https://www.mouser.com/new/doodle-labs/doodle-labs-rm915-rm-2450-smart-radios/.

Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.

Acerca de Mouser

2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.

Acerca de Doodle Labs

2026 - Doodle Labs desarrolla innovadores transceptores de banda ancha inalámbricos y subsistemas frontales (FES) para aplicaciones de IoT industriales. Durante más de 18 años, los fabricantes OEM han confiado en Doodle Labs por su experiencia en el diseño de sus sistemas inalámbricos. Su filosofía de diseño se enfoca en lograr el mejor desempeño de su clase, a la vez que requiere un mínimo esfuerzo de integración, lo que les permite a los clientes ingresar al mercado con mayor rapidez con mejores productos a un costo general más accesible. www.doodlelabs.com.

Marcas

Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.

Para obtener más información, comuníquese con:
Kevin Hess, Mouser Electronics
Vicepresidente general de Marketing
+1 (817) 804-3833
Para consultas de prensa, comuníquese con:
Kelly DeGarmo, Mouser Electronics
Gerente, Comunicaciones Corporativas y Relaciones con los Medios
+1 (817) 804-7764