Infineon ICL5101 Resonant Controller IC with 650V High-Side Driver Now at Mouser
April 13, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now stocking the ICL5101 LED Resonant Controller IC from Infineon Technologies. Integrating a half-bridge controller with a Power Factor Correction (PFC) stage in a single package, the ICL5101 extends Infineon's existing portfolio of lighting control ICs to address lighting systems in the range of 40Watts to 300Watts. The high level of integration ensures a low count of external components, enabling small form factor designs that are ideal for compact power supplies in lighting applications such as an LED driver.
The Infineon ICL5101 LED Resonant Controller IC, available from Mouser Electronics, includes both a half-bridge controller and a PFC stage. The PFC stage operates in CrCM and DCM mode, allowing LED lighting to be dimmed from 100 percent down to an extremely low 0.1 percent of its nominal power load without audible noise. The half-bridge resonant stage provides high- and low-side gate drive functionality for discrete MOSFETs rated up to 650V, and features a self-adaptive dead time control of the half-bridge driver from 500ns to 1.0µs. Other features of the resonant half bridge controller include improved operation control in magnetic saturation during start-up, and advanced error detection.
The Infineon ICL5101 LED Resonant Controller provides an ultra-fast time-to-light of less than 200ms under any conditions, and a high efficiency of up to 94 percent. The device is extremely stable over line voltage variations, and is equipped with a comprehensive set of protection features including external over temperature protection, overload protection, short circuit protection, and capacitive load protection to increase system safety. All operation parameters of the IC, including protection features, are adjustable by using external resistors, making this chip an ideal choice for reliable systems that are easy to design by using approximately 25 percent fewer components compared to similar solutions which require separate PFC and resonant ICs.
The ICL5101 LED Resonant Controller supports outdoor use by an extended junction temperature ranging from -40°C to 125°C, and is available through Mouser Electronics in a compact, PG-DSO-16-pin package. The device is targeted toward a variety of lighting applications, including Indoor/outdoor high-power LED lighting; high-bay/low-bay lighting; street lighting; parking garages and area lighting; and office/shop lighting.
To learn more, visit:
http://www.mouser.com/new/Infineon-Technologies/infineon-icl5101-controller/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.
2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.
2026 - Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. Infineon semiconductors enable efficient energy management, smart mobility, and secure, seamless communications in an increasingly connected world.
Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.