Amphenol FCI Millipacs High-Speed Right-Angle Receptacles Now at Mouser Electronics
January 10, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Millipacs® high-speed right-angle receptacles from Amphenol FCI.
Part of Amphenol FCI's Millipacs 2.0 mm wire-to-board and board-to-board interconnect system, the high-speed right-angle receptacles support data rates up to 25 Gbps. These receptacles also support mating compatibility with IEC 61076-4-101 series 2mm hard metric (HM) backplane headers. The Millipacs high-speed receptacle and standard 2 mm hard metric vertical header mating combination features low-crosstalk performance at higher frequencies.
Millipacs receptacles are offered in a 5-row version which provides up to 24 differential pairs (DP) for Type A or 30 DP for Type AB per 50 mm of standard module length. Available models include both broad-side coupling (horizontal row-wise pinning) and edge-side coupling (vertical column-wise pinning). This flexibility allows users upgrade to higher data rates while retaining existing vertical headers in backplane and the backplane system architecture. The Amphenol FCI Mllipacs high-speed receptacles are suitable for a applications within the medical, data, industrial, instrumentation, and communication fields.
For more information, visit www.mouser.com/amphenol-fci-millipacs-high-speed-receptacles.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 750 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Amphenol FCI
Amphenol FCI (Amphenol ICC) designs and manufactures a wide array of high-tech connector solutions for various market applications, including data-communications and telecommunications, data storage and servers, consumer electronics, medical, industrial and instrumentation, automotive motorized vehicles as well as renewable energy.
Amphenol Corporation acquired FCI Asia Pte Ltd., further strengthening FCI as an international connector and cable assembly solutions manufacturer of backplane connectors, power solutions, board-to-board and wire-to-board connectors, input/output connectors, optical interconnect, cable assemblies and flex connectors.
AFCI is well renowned and respected for their technological leadership as well as innovative connector and cable assembly solutions.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com