Wolfspeed’s High-Efficiency GaN HEMTs for RF Power Amps Now Shipping from Mouser Electronics

Anuncio de nuevos productos

Comuníquese con nosotros


Wolfspeed’s High-Efficiency GaN HEMTs for RF Power Amps Now Shipping from Mouser Electronics

February 28, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the CG2H40xx and CG2H30070 gallium-nitride (GaN) high-electron-mobility transistors (HEMTs) from Wolfspeed™, a Cree® company. Operating from a 28-volt rail, the two HEMTs offer a versatile, general-purpose broadband solution for a variety of radio frequency (RF) and microwave applications. Wolfspeed's reliable HEMTs are characterized by high efficiency, high gain and wide bandwidth, making them an ideal choice for linear and compressed amplifier circuits.

The Wolfspeed CG2H40xx and CG2H30070 GaN HEMTs, available from Mouser Electronics, offer best-in-class reliability and a choice of two package types: a screw-down flange package or solder-down pill package. Designed with the same footprint as previous 0.4µm devices, the new HEMTs can be used as drop-in replacements in existing applications. The transistors are capable of high frequency operation to 6 GHz and deliver 62-percent efficiency at PSAT.

The high efficiency and wide bandwidth of Wolfspeed's CG2H40xx and CG2H30070 GaN HEMTs enables RF design engineers to increase the performance of their RF amplifiers quickly and easily. The transistors are an ideal option for a broad range of RF power amplifier applications, ranging from military communications and radar equipment to commercial RF applications in industrial, medical and scientific industries.

The CG2H40xx and CG2H30070 GaN HEMTs from Wolfspeed are supported by the CG2H4004F-TB and the CG2H30070F-TB1 demonstration boards, which allow engineers to efficiently evaluate the Wolfspeed HEMTs. The CG2H4004F-TB development tool operates at a frequency range of DC to 4 GHz, while the CG2H30070F-TB1 development tool operates at a frequency range of 0.5 GHz to 3 GHz.

To learn more, visit www.mouser.com/wolfspeed-cgh2400-cgh300-hemt.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Como distribuidor autorizado a nivel global, Mouser ofrece la más amplia selección de los semiconducoctores y componentes electrónicos más recientes del mundo, en existencia y listos para enviar. Los clientes de Mouser pueden esperar productos originales y 100 % certificados que son totalmente localizables desde cada uno de sus socios fabricantes. Para ayudar a agilizar los diseños de los clientes, el sitio web de Mouser cuenta con una amplia biblioteca de recursos técnicos, incluso un Centro de recursos técnicos, además de documentos técnicos de productos, diseños de referencia de proveedores específicos, notas de aplicación, información técnica de diseño, herramientas de ingeniería y otro tipo de información útil.

Acerca de Mouser

2026 - Mouser Electronics es un distribuidor autorizado de semiconductores y componentes electrónicos que se enfoca en introducir nuevos productos de sus socios fabricantes líderes. Debido a que brinda servicios a la comunidad global de compradores e ingenieros de diseño electrónico, el sitio web global del distribuidor, mouser.com, está disponible en múltiples idiomas y monedas, y cuenta con más de 6,8 millones de productos de más de 1.200 marcas de fabricantes. Mouser ofrece 28 ubicaciones de asistencia en todo el mundo para ofrecer el mejor servicio al cliente de su clase en idiomas, monedas y horarios locales. El distribuidor realiza envíos a más de 650.000 clientes en 223 países o territorios desde sus innovadoras instalaciones de distribución de 93.000 metros cuadrados en el área metropolitana de Dallas, Texas. Para obtener más información, visite https://www.mouser.com.

Acerca de Wolfspeed

2026 - Wolfspeed (NYSE: WOLF) leads the market in the worldwide adoption of silicon carbide (SiC) technologies. Wolfspeed provides industry-leading solutions for efficient energy consumption and a sustainable future. Wolfspeed’s product families include SiC materials and power devices targeted for various applications, such as electric vehicles, fast charging, and renewable energy and storage. Through the power of SiC, Wolfspeed is powering a cleaner, safer, cooler, greener world.

Marcas

Mouser y Mouser Electronics son marcas registradas de Mouser Electronics, Inc. Todos los demás productos, logotipos y nombres de empresas mencionados en este documento pueden ser marcas de sus respectivos titulares.

Para obtener más información, comuníquese con:
Kevin Hess, Mouser Electronics
Vicepresidente general de Marketing
+1 (817) 804-3833
Para consultas de prensa, comuníquese con:
Kelly DeGarmo, Mouser Electronics
Gerente, Comunicaciones Corporativas y Relaciones con los Medios
+1 (817) 804-7764